WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability

Eco-efficiency and Waste and Emission Management

Circular and efficient operations

The circular economy seeks to maximize the value of resources while minimizing waste and environmental impacts. In this model, products are designed to be durable, repairable and recyclable, encouraging the reuse and recycling of materials. Instead of following the traditional linear model of production and consumption, in which products are manufactured, used and discarded, the circular economy promotes the idea of a continuous cycle, where materials are kept in use for as long as possible.

This approach not only contributes to the conservation of natural resources but also stimulates innovation, job creation and sustainable economic growth, making it essential to address today's global challenges such as climate change and resource scarcity.

Consolidating WEG's commitment, we have ISO 14,001 certifications demonstrating environmental management in the company's operations.

Programs & Practices

Residues and energy

Solid residues

WEG operations have a selective waste collection system. In this way, residues are separated and sent to recyclers of each material, enabling their appreciation and the reintroduction of such materials in different production cycles. It is important to emphasize that part of the waste generated in the operations is recycled by WEG itself, returning to the process and forming part of its products. All waste is sent to environmentally responsible companies, selected and developed by WEG's environmental management team.

See more

 

Energy

WEG has had an Energy Efficiency Policy since 2012, showing its commitment to the management of this input. This policy is deployed into actions to monitor and reduce energy consumption, which contributes to improving the environment. WEG intends to increasingly make its energy sources cleaner, renewable and sustainable.

Water, effluents and water resources

WEG monitors the water consumption of its operations and has several operational controls that ensure efficient management of this resource, thus avoiding waste and promoting conscious consumption. All effluents generated in operations are properly treated and periodically monitored in order to ensure compliance with legislation and minimize impacts on different stakeholders.

 

Part of the effluents treated in the operations are reused in the internal processes, where some effluent treatment plants enable the reuse of up to 100% of the treated effluent. We have adopted initiatives focused on reducing water consumption and effluent generation by controlling leaks, monitoring consumption and counting on the support of programs that engage all employees in this objective, such as KaizenWEG and WEG Manufacturing System.

 

Investments and expenses in the environment

Environmental investments fall into three categories:

  • Environmental control: related to treatment and disposal of residues, treatment of atmospheric and liquid emissions, environmental liability insurances, depreciation of devices and expenses with materials and maintenance.
  • Equipment: related to the purchase of equipment for environmental control.
  • Management: related to the remuneration of training staff who act in environmental management, research and development, and certification of environmental management systems.

Embalagens sustentáveis e preservação da biodiversiade

Possuímos uma fábrica de embalagens, a RF Reflorestadora, localizada no Brasil.

Essa unidade produz todas as embalagens de madeira utilizadas em nossas diversas linhas de produto. Para isso, contamos com áreas de reflorestamento próprias que garantem o fornecimento contínuo de madeira e a preservação desse recurso natural e de áreas de florestas naturais, reserva legal e áreas de preservação permanente que ajudam na conservação da biodiversidade local.

As áreas atendem todas legislações e requisitos legais, bem como uma área de conservação de florestas nativas muito superior ao mínimo da reserva legal estabelecida.

Além disso, a WEG promove e apoia iniciativas de reflorestamento consciente e conservação da natureza e investe na arborização de seus parques fabris.

Kaizen WEG

O KaizenWEG é uma das formas de gestão participativa da WEG, onde todos os colaboradores são incentivados a promover melhorias em seu ambiente de trabalho ou em quaisquer outras áreas da empresa, identificando desperdícios, analisando causas e participando de equipes de implantação de melhorias.

A busca coletiva pela excelência operacional e sustentabilidade em um cenário de verticalização de processos faz da gestão participativa peça chave para a potencialização dos resultados da WEG.

Média de 2019 a 2021: 1.144

WMS

O sistema de gestão de melhoria contínua da WEG é o WMS, que tem como principal objetivo a identificação e eliminação de perdas e desperdícios.

Os resultados são maximizados através das matrizes de priorização de segurança, qualidade, custo e emissões de GEE (gases de efeito estufa), que direcionam a ocorrência de projetos de otimização ou eliminação destes desperdícios, contribuindo para um mundo mais eficiente e sustentável.

Além das frentes de trabalho de otimização, times multidisciplinares atuam como pontos focais de melhoria contínua, trazendo inovações e disrupções nos nossos processos.

Um destes pontos focais é o pilar de Meio Ambiente e Energia, que objetiva e sistematiza a redução de impactos ambientais, atuando para reduzir ou eliminar a geração de resíduos e emissões, o consumo de recursos energéticos, limpezas químicas e insumos em geral.

Saiba mais

 

Plano de troca

Reciclagem é assunto sério para a WEG, estendido até o seu negócio. Com o programa de reaproveitamento de motores elétricos, “Plano de Troca”, a companhia concede um desconto na compra de um motor novo com rendimento superior ao exigido por lei na troca por um usado. Além do benefício financeiro aos clientes, a iniciativa garante que o motor usado com baixo nível de eficiência seja removido de uso. Depois de recolhidos pela companhia, os motores são desmontados e separados em peças para envio a recicladores credenciados e rastreados.

 

Vantagens

  • Redução do consumo de energia elétrica

  • Confiabilidade da planta

  • Redução dos custos operacionais

  • Garantia de fábrica

  • Produtos normalizados – oferecem total intercambiabilidade com motores já instalados

 

Item

2019

2020

2021

2022

2023

Produtos vendidos que podem ser reutilizados ou reciclados* (%) – Base em peso

65

66

68

73

65

Produtos que foram realmente reaproveitados ou reciclados pela empresa * (%) – Base em peso

21

13

8

5

4,3

* Leva em consideração somente os produtos colocados e recolhidos no mercado Brasil

 

Investimentos em meio ambiente

Os investimentos ambientais são caracterizados em três categorias:

Controle ambiental: Relacionado com tratamento e disposição de resíduos, tratamento de emissões atmosféricas e líquidas, seguros de responsabilidade ambiental e depreciação de equipamentos e despesas com materiais e serviços de manutenção.

Equipamentos: Relacionados à aquisição de equipamentos para controle ambiental.

Gestão: Relacionado à remuneração de profissionais de treinamento que exercem atividades de gestão ambiental, pesquisa e desenvolvimento, certificação de sistemas de gestão ambiental.

Abaixo o montante investido em cada categoria no Brasil :

Investimento

2021
Valor em R$ Mil

2021
(%)

2022
Valor em R$ Mil

2022
(%)

2023
Valor em R$ Mil

2023
(%)

Controle Ambiental

8.678

54,19

10.234

52,4

12.248

48,4

Equipamentos

1.329

8,30

1.788

9,2

1.819

7,2

Gestão  6.006 37,51 7.519 38,5 11.261 44,4
 TOTAL 16.013 100 19.540 100 25.328 100

 

Certificação Ambiental

Em 2023, considerando o escopo de colaboradores, 74,5% do grupo WEG estava coberto pela certificação ISO 14001.

Clique aqui para acessar nossos certificados

 

Auditorias Ambientais

A WEG possui um processo de ciclo de auditorias ambientais que cobre todas as suas operações industriais.

Dentro do seu processo anual de auditorias ambientais, a WEG garante o atendimento às legislações ambientais de todas as suas operações industriais.

 

Indicadores de Performance

Em 2023, o escopo das unidades monitoradas foi ampliado, incluindo os endereços comerciais da empresa. Dessa forma, 100% dos endereços globais da WEG agora estão contemplados nos indicadores.

 

Resíduos Sólidos

A WEG possui um sistema de coleta seletiva de resíduos em suas operações. Os resíduos são separados e enviados para os recicladores, possibilitando assim a valorização desses e a reintrodução dos materiais nos mais diversos ciclos produtivos. Parte dos resíduos gerados nas operações também são reciclados pela própria WEG, retornando assim ao processo e fazendo parte dos nossos produtos.

 

Itens

Unidade

2019

2020

2021

2022

2023

Total de resíduos perigosos reciclados/reutilizado

Toneladas métricas 

0 0 0

0

3.101

Total de resíduos perigosos descartados

Toneladas métricas    5.822

4.905

5.484 

6.511

5.944

Resíduos perigosos depositados em aterro

Toneladas métricas   1.266

1.338

1.138

850 0

Resíduos perigosos incinerados com valorização energética

Toneladas métricas   0  0 0 0 0
 Resíduos perigosos incinerados sem valorização energética Toneladas métricas   4.556  3.567 4.346 5.661 5.944

Resíduos perigosos com método de disposição desconhecido 

Toneladas métricas   0  0 0 0 0
 Cobertura de dados (como % do denominador) % de empregados  100 100 100 100 100

 

Energia

A WEG possui Política de Eficiência Energética, desde 2012, na qual demonstra o seu compromisso com a gestão desse insumo. Essa política é desdobrada em ações para o monitoramento e a redução do consumo de energia, o que contribui para a melhoria do meio ambiente. A WEG pretende tornar, cada vez mais, suas fontes de energia mais limpas, renováveis e sustentáveis.

Consumo total de energia

Unidade

2019

2020

2021

2022

2023

Consumo total de energia Não-Renovável

MWh

466.737 462.976 499.355

478.872

430.848

Consumo total de energia Renovável

MWh 0

0

56.000

86.918

127.709

Consumo total de energia (Não-Renovável + Renovável)

MWh 466.737

462.976

555.355

565.790 558.557

Dados de cobertura (%)

Em relação à funcionários

100 100 100 100 100

Aquisição de energia renovável

Em 2023, a WEG garantiu que 22,9% do consumo de energia fosse proveniente de fontes renováveis com garantia de origem por meio autoprodução, compra de certificados de energia renovável (I-REC)e contratos bilaterais.

A WEG em 2024 terá aproximadamente 90% do consumo elétrico do Brasil de fonte renovável, sendo que esse valor equivale a 45 MW médio.

 

Emissões Atmosféricas

A WEG realiza o monitoramento das emissões atmosférica relacionadas aos compostos orgânicos voláteis. Abaixo segue o resultado das emissões relacionadas aos equipamentos monitorados nos últimos anos.

 

Item

2019

2020

2021

2022

2023

Emissões de compostos orgânicos voláteis - VOC (t/ano)

93,5 135,2 114,5

139,3

382,6

Taxa de cobertura (%)

56

56

56

61

72

 

Violações Ambientais

Uma das principais prioridades da WEG é a conformidade com a legislação ambiental aplicável às suas operações. Nos últimos 4 anos, não houve evidências de multas ambientais aplicadas aos negócios da WEG.

Sepa más sobre las acciones de WEG en Sustentabilidad

Asociación entre Natura, WEG y ATAIC inaugura agroindustria alimentada por energía solar en la Amazonía

Asociación entre Natura, WEG y ATAIC inaugura agroindustria alimentada por energía solar en la Amazonía

Instalación de sistema fotovoltaico con almacenamiento en baterías amplía la autonomía energética y la productividad de 470 familias agro extractivistas en Ilha das Cinzas, en Pará

Hotel & SPA frente al mar en el noreste de Brasil será alimentado por transformador encapsulado en seco de WEG

Hotel & SPA frente al mar en el noreste de Brasil será alimentado por transformador encapsulado en seco de WEG

Reconocido por su eficiencia energética y confiabilidad, el transformador seco es la opción ideal para aplicaciones en el segmento de infraestructura

WEG publica su Informe Anual Integrado, reforzando su compromiso con la sostenibilidad

WEG publica su Informe Anual Integrado, reforzando su compromiso con la sostenibilidad

La compañía presenta avances significativos en diversas áreas

WEG suministra hidrogeneradores para proyecto en Portugal

WEG suministra hidrogeneradores para proyecto en Portugal

Los hidrogeneradores fortalecerán la producción de energía renovable en la central hidroeléctrica

WEG impulsa el Proyecto Sucuriú, la primera fábrica de celulosa blanqueada de Arauco en Brasil

WEG impulsa el Proyecto Sucuriú, la primera fábrica de celulosa blanqueada de Arauco en Brasil

Soluciones tecnológicas de WEG refuerzan la eficiencia, confiabilidad y sostenibilidad en el sector de celulosa

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Teléfono: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability