WEG
  • Index
  • Products
    • SUSTAINABLE PRODUCTS AND SOLUTIONS
    • Technologies and Innovation for Energy Transition and Decarbonization
    • Responsible supply chain
  • Operations
    • CIRCULAR AND EFFICIENT OPERATIONS
    • Eco-efficiency and Waste and Emission Management
    • Carbon Neutral in Operations
  • People
    • ENGAGED EMPLOYEES AND COMMUNITIES
    • Sustainable Growth of the Communities
    • Comprehensive Well-being, Diversity and Inclusion
  • Governance
    • GOVERNANCE AND ETHICAL CONDUCT
    • Engagement and Transparent Communication
    • Compliance and Integrity
WEG - Driving efficiency and sustainability
 

Technologies and Innovations for Energy Transition and Decarbonization

Through the company's strategic direction for its business model, WEG has, in all its business units, more efficient solutions and products with less environmental impact, such as renewable energy (solar and wind power), electric mobility and energy efficiency. WEG develops products considering strict risk criteria related to health and safety. In the development phase, analyzes such as Quality Function Deployment (QFD) and Risk Assessment are applied.

Below are some highlights, considering the variety of products and solutions that the company provides to the market through its different business units.

Energy and Industrial Efficiency

W51 HD Motor (High Density)

Efficient and compact solution thar delivers high performance with reduced size and weight in comparison to the previous line (up to 25% higher power density – kW/kg) and its competitors. Therefore, it makes rational use of raw materials in the manufacture of motors and reduces the potential effects of their transformation, cutting down GHG emissions by about 15% in comparison to the previous line.

VSD for Motors

High-tech VSD for driving and controlling three-phase induction and permanent magnet motors. Thanks to its technology, this VSD model provides energy savings, safety, increased productivity and quality in the process network in which it is implemented. The CFW900, together with permanent magnet motors, offers the highest energy efficiency solution on the market. The new HMI with Bluetooth® connectivity is ideal for panel builders and repair shops, enabling programming, monitoring, parameter backup and other functionalities via tablets or smartphones.

BLDC Motor Line (Brushless DC)

For application in front load washing machines, it delivers a 60% improvement in the performance of the operating cycle and, consequently, a reduction of GHG emissions during the operation phase. This line currently represents 20% of the volume sold by WEG for front load washing machines.

Renewable Energy

Wind Power

In July 2022, WEG announced the release of a new wind turbine platform with 7 MW power and 172 meters of blade rotor diameter. This wind turbine will become the largest machine in operation in the Brazilian market. More powerful and efficient, the new model brings greater generation to wind projects.

Solar Power

WEG established itself as one of the main suppliers of products and solutions for solar plants in Brazil, bringing efficiency that drives sustainability in cities, industries, agribusiness and homes across the country. WEG has a vast portfolio of products for all the stages of photovoltaic solar generation projects, with solutions for the energy conversion and internal distribution system, from the plant to the point of connection to the electrical system through high voltage substations.

Hydroelectric Generation

WEG was selected to supply the generators for São Roque Hydroelectric Power Plant, located in the city of Vargem-SC. The generators are one of the most important parts of the enterprise for São Roque Hydroelectric Power Plant. With 285 tons each and approximately eight meters in diameter, this equipment is among the largest electric hydrogenerators ever produced by WEG.

São Roque Hydroelectric Power Plant has an installed capacity of 142 MW, which, on average, is enough to supply a city with approximately 170,000 inhabitants. The generators started commercial operation in July 2022.

Commercial and Industrial Energy Storage

Energy storage systems are used in commercial or industrial facilities, being the complete solution for storage and management of electrical energy. They can be configured to perform various functions in smart systems for generation, transmission and distribution of electric energy. The system is composed of an energy control and management solution, and it is mainly recommended for applications in systems installed behind the meter in industries, stores, shopping malls, residential condominiums and electric mobility infrastructure.

Transformadores para Energias Renováveis

A confiabilidade dos transformadores desenvolvidos para usinas solares tem como objetivo a garantia do fornecimento de energia, permitindo acesso à eletricidade por meio de fontes de geração de energia renovável. Na linha de transformadores para usinas eólicas, a WEG desenvolveu projeto elétrico e mecânico do transformador extremamente compacto. Adicionalmente, pela configuração da instalação, na qual a fonte e a unidade transformadora encontram-se muito próximas entre si, o sistema possibilita menos perdas e mais eficiência energética.

Mobilidade Elétrica

Soluções integradas para veículos elétricos

A WEG desenvolve continuamente tecnologias inovadoras para criar sistemas de tração elétrica, bem como toda a infraestrutura elétrica necessária para operação de veículos elétricos. Os sistemas de tração elétrica WEG podem ser aplicados em diversos veículos rodoviários, ferroviários e de navegação, tais como caminhões e ônibus urbanos, furgões, empilhadeiras elétricas, trens, monotrilhos, navios de suporte e rebocadores.

Soluções Digitais

Sistemas inteligentes e sustentáveis

Sistemas inteligentes são capazes de integrar os mais variados dispositivos e máquinas, bem como instalações e processos, promovendo eficiência na tomada de decisão e aumento da eficiência operacional. Soluções e sistemas mais inteligentes também promovem a utilização mais eficiente de recursos energéticos ajudando a reduzir pegada de carbono das operações em todos os níveis.

Automation Systems

WEG supplies completely integrated control systems that guarantee high performance of industrial processes, easy operation and productivity gains by means of state-of-the-art technology. The success of the integration of this system is in the synergy of WEG products, where motors, drives, generators, electric panels and software applications are integrated, providing the ideal solution for each requirement. The control of industrial processes requires automation systems with high reliability and uptime levels, in addition to easy asset management by the maintenance teams, extending the equipment service life and streamlining the use of resources.

WEG Transformer Fleet Management and WEG Power Transformer Specialist

WEG Transformer Fleet Management is the ideal solution to monitor online and manage the fleet of oil or dry-type transformers, enabling customers to maximize the efficiency of their operations, supporting the streamlined management of industrial plants, renewable energy generation and infrastructure. WEG Power Transformer Specialist is a digital solution used to monitor and manage power transformers that, integrated with the WEG Transformer Fleet Management platform, centralizes the signals from several sensors installed on the equipment.

WEG Motion Fleet Management

Developed to simplify and speed up the operation, maintenance and management of industrial plants, WEG Motor Fleet Management is the ideal solution for monitoring and increasing the uptime of the industrial drive fleet. Based on cloud computing technology, the performance of assets can be monitored at any time, from any part of the world. WEG Motor Fleet Management allows checking the operating status of low and medium voltage motors and drives (VSDs and soft-starters), gearboxes, gearmotors, compressors and other assets installed in any kind of industry or facility.

Ultra Low Bake (ULB) Technology for Coatings

The Ultra Low Bake (ULB) technology consists of reducing the curing time or curing temperature of powder coatings. Linked to this reduction in time or temperature (which can reach up to 35%) is the reduction in the amount of gas used in the curing ovens of customers and partners, lowering GHG emissions.

WEG partners who employ such technology in their production line, in addition to reducing environmental impact, have a significant increase in productivity and competitiveness. WEG has forty products developed for this purpose.

Material efficiency and environmental assessment of the product

In its value chain, WEG adopts initiatives in line with the principles of the circular economy, using practices that include the reuse of process residues as raw material, like stamping steel scrap used to make castings, and the adoption of programs to recover materials at the end of the product life cycle through reverse logistics and replacement plans.

The application of these concepts and practices allowed WEG to achieve a material efficiency rate close to 85%. WEG is also constantly improving and evolving the energy efficiency of its products and retrofit solutions to extend the service life of some product lines. Qualified teams work on the processes to develop new products, on the design of new lines and in the implementation of more efficient industrial processes.

WEG applies the LCA (Life Cycle Analysis) to generate the EPD (Environmental Product Declarations) according to the customers’ demands, intending, in the coming years, to expand the application of these tools.

Saiba mais sobre as ações da WEG em Sustentabilidade

Parceria entre Natura, WEG e ATAIC inaugura agroindústria movida à energia solar na Amazônia

Parceria entre Natura, WEG e ATAIC inaugura agroindústria movida à energia solar na Amazônia

Instalação de sistema fotovoltaico, com armazenamento de energia em baterias, amplia autonomia energética e produtividade de 470 famílias agroextrativistas na Ilha das Cinzas, no Pará

Hotel & SPA beira-mar na região nordeste do Brasil será alimentado por transformador a seco encapsulado WEG

Hotel & SPA beira-mar na região nordeste do Brasil será alimentado por transformador a seco encapsulado WEG

Referência em eficiência energética e confiabilidade, o transformador seco é a escolha ideal para aplicações no segmento de infraestrutura

WEG divulga Relatório Anual Integrado, reforçando compromissos com a sustentabilidade

WEG divulga Relatório Anual Integrado, reforçando compromissos com a sustentabilidade

Companhia apresenta avanços significativos em diversos aspectos

WEG fornece hidrogeradores para projeto em Portugal

WEG fornece hidrogeradores para projeto em Portugal

Os hidrogeradores irão fortalecer a produção de energia renovável na central hidrelétrica

WEG impulsiona o Projeto Sucuriú, primeira fábrica de celulose branqueada da Arauco no Brasil

WEG impulsiona o Projeto Sucuriú, primeira fábrica de celulose branqueada da Arauco no Brasil

Soluções tecnológicas da WEG reforçam eficiência, confiabilidade e sustentabilidade no setor de celulose

Grupo WEG
  • Avenida Prefeito Waldemar Grubba, 3300 - 89256-900 - Jaraguá do Sul - SC
  • Telefone: +55 47 3276 4000
  • E-mail: esg@weg.net






 

Instagram LinkedIn YouTube

 



 
WEG - Driving Efficiency and Sustainability