Retornar para Minha Conta
A WEG, através da sua unidade de Tintas, está atuando há mais de 30 anos no fornecimento de soluções em proteção a corrosão através de tintas industriais e anticorrosivas, atendendo vários fabricantes de máquinas, equipamentos e estruturas metálicas, com ótimas referências no segmento de mineração e ampla rede de técnicos em pinturas do Brasil. Para atender as diferentes exigências nos processos de extração, beneficiamento e transporte de minérios, as tintas WEG tem por objetivo evitar acidentes com corrosão, diminuir os gastos com manutenção na pintura e evitar paradas não programadas, garantindo maior produtividade.
As diversas características encontradas durante a extração dos minerais, nas indústrias de beneficiamento e nos processos de movimentação, como a exposição a agentes químicos e corrosivos, ambientes com alta umidade, associada ao poder abrasivo, geram necessidade por materiais e revestimentos de alta performance.
Excess dust in the extraction, crushing, sieving, grinding and handling of ore and cement is inherent, in many situations the extraction occurs in humid environments. This means that the coatings on the machines, equipment, conveyor belts and metal structures must be highly resistant, easy to apply and cost effective.
WEG double-function epoxy line, together with the polyurethane topcoat meet the requirements for these processes and are recommended for construction through to maintenance.
During production, the use of separation techniques based on gravity, flotation or leaching exposes equipment to continuous contact with liquids, often in extremely aggressive environments. Pipes and metal frames that are buried or submerged in fresh or salty water also require protective coatings.
WEG’s technologically advanced resins ensure excellent performance as indoor or outdoor coatings for pipes, storage and mixing tanks, flotation columns and cells, decanters, dewatering systems, thickeners, clarifiers and filters.
Some products and materials used in the processing units are corrosive. So the equipment, tanks, pipes and structures that remain in touch with these chemicals need protection. WEG has product lines developed to withstand conditions such as the transportation and storage of fertilizers, inputs, acids and bases; mixing equipment and mineral electrolytic extraction equipment.
Shipping ports where materials are loaded or received are continuously subject to salt spray and humidity, creating one of the most corrosive environments. Factories and processing units in areas with a high concentration of pollutants are also subject to highly aggressive conditions for machinery to operate under.
Contact us and we will be glad to answer your questions