WEG is committed to the safety, maintenance and improvement of the quality of life of its employees, providing a safe and healthy environment for daily activities.
Some of the programs and actions that promote health, well-being and quality of life: Living Well Program, Vaccination Campaigns, Labor Gymnastics, Occupational Health and Medical Surveillance Program, Ergonomics Program and WEG Hearing Conservation Program.
Some of the programs and actions that promote safety: LTFIR Reduction Goal, Routines for Mapping Safety and Ergonomics Hazards and Risks, Safety Audits, Internal Accident Prevention Commission, Machine and Equipment Assessment Program etc.
WEG also has training and awareness initiatives on global health issues, such as HIV/AIDS, Tuberculosis and Chronic Noncommunicable Diseases – NCDs (e.g. hypertension, diabetes, etc.)
In addition to those programs and actions, WEG offers various benefits to employees, such as Health Plan, Dental Plan, WEG Social Security, gifts on commemorative dates etc.
In 2023, WEG launched an awareness campaign about the use of cell phones, warning about the risks involved when these devices are used on the move.
WEG operations, according to the needs and definitions of each location/country, have benefits that provide a balance between personal and professional life, such as:
At WEG, organizational climate management consists of the stages of investigation, diagnosis, action plans, implementation and monitoring.
The Internal Organizational Climate Survey is a tool that indicates employees' perception of the company's climate and their engagement and satisfaction through data collection. It is implemented in all units in Brazil and is expanding to branches abroad.
Based on the results, strategies and actions are outlined to build a more inclusive, innovative and high-performance environment. Action plans are developed by leaders to meet specific needs and a corporate plan meets common needs between different areas and locations.
The result is evolving with each cycle, the result of joint work between managers and all employees. The Internal Organizational Climate Survey revealed in 2022 an increase of 11% in the level of satisfaction, reaching a total of 78.8%.
As a highlight in people management, WEG has received external recognition as "a place where everyone wants to work" (employer of choice). Mexico has been recognized for 12 years with the Super Empresas Expansión award. In 2024, she was recognized again in this award.
The WEG Code of Ethics plays an important role in establishing the conduct expected from our employees and other stakeholders, as well as in reinforcing WEG's commitment to promoting a culture of respect for others.
Entendendo a importância do papel das lideranças para a Diversidade e Inclusão a WEG possui um módulo de treinamento na Academia de Lideranças, dedicado ao tema.
A Academia de Lideranças da WEG faz parte do Programa Desenvolvimento de Chefia, cujo objetivo é proporcionar aos novos líderes a imersão na cultura WEG e destacar a importância do seu papel no processo de gestão de pessoas.
Além do módulo de treinamento na Academia de Lideranças, palestras e workshops vem sendo realizados para engajamento e sensibilização de gestores.
O treinamento no Código de Ética WEG, que contempla todos os colaboradores, também engloba questões de Diversidade, Equidade e Inclusão.
Atenta a los desafíos y necesidades de evolución continua en diferentes frentes de diversidad e inclusión, WEG viene desarrollando importantes iniciativas para evolucionar la gestión de inclusión de personas con deficiencia.
El programa QPcD - Cualificación para personas con Deficiencia tiene el objetivo de capacitar y desarrollar a los candidatos PcDs para una actuación en actividades operacionales.
Algunos ejemplos de acciones para diversidad e inclusión ya implementadas:
En Brasil, todos los empleados están cubiertos y regidos por normas colectivas, mientras que los empleados del exterior que pueden no estar cubiertos tienen contratos y condiciones de trabajo basados en la legislación laboral local, que se respeta en su totalidad.
Además de Brasil, los empleados de las operaciones en China, Sudáfrica, México, India y España también se rigen por convenios colectivos, lo que representa aproximadamente el 87% de los empleados de WEG en todo el mundo.
WEG ofrece programas de educación y capacitación que incluyen capacitación técnica y comportamental, con el objetivo de proporcionar una mayor cualificación a sus colaboradores y generar estrategias más competitivas al mercado. Eso es fundamental tanto para el buen desempeño y desarrollo profesional de los colaboradores como para contribuir y atender las expectativas de crecimiento continuo y sustentable de la organización.
Toda capacitación de los colaboradores es direccionada a las necesidades del cargo actual o para el cargo que el colaborador está siendo preparado para ejercer en el futuro.
Para auxiliar a los colaboradores en su desarrollo y en su carrera, WEG tiene programas de elevación, desarrollo y de cualificación, como por ejemplo: QPOP - Cualificación profesional de operadores de producción, QPET - Cualificación profesional de ingenieros y tecnólogos, QPSS - Cualificación profesional en six sigma, Academia de liderazgos, posgraduaciones in company, auxilio escolar, capacitaciones internas, etc.
En 2023, el 62% de las vacantes en WEG fueron cubiertas por candidatos internos.