The eleven three-phase induction motors, suitable for operation in explosive atmospheres will be used to drive the centrifugal pumps feeding water into the cooling towers at the Petrobras Abreu e Lima Refinery in Ipojuca, Pernambuco. This is one of the wealthiest regions of Brazil, and close to the world famous beach resorts of Porto de Galinhas.
The pumps and motors are to be located in the refining area and will be used to feed the cooling towers associated with the site’s main steam turbines. The pumps will operate to provide water for circulation and for cooling the plant and equipment which is critically important within the refining process. The pumps are being supplied by KSB, which has been manufacturing in Brazil for over 50 years.
“These KSB pumps and associated equipment require special motors that offer a high degree of reliability,” explains WEG engineer, Marcelo Vedana. To enhance their reliability the motors are designed to be robust and use the best quality bearings and ancillary components. The windings are precision made and balanced, whilst advanced thermal management ensures cool running.
Explosion proof motors are designed to contain an explosion if it occurs within the motor. This is to prevent the release of explosive gases and to minimize internal sparking within the motor. They are most commonly used in the chemical, mining, textile and petrochemical industries, but also find applications in many other fields. Not only must an explosion proof motor be designed to reduce the likelihood of exploding, it must also be capable of completely containing an internal explosion so that it does not propagate to the surrounding area. Thus their bodies tend to be more robust than standard motors and to be able to maintain integrity at highly elevated temperatures. They must also resist corrosion and to have flame-tight joints and flanges with minimum tolerances so that hot gases from an internal explosion will cool down before exiting to the wider environment.
There are several approval bodies that can certify motors are explosion proof. As a major international motor manufacturer, WEG meets the safety requirements for all regions. Petrobras, amongst the five biggest energy companies in the world, says that Abreu e Lima is one of the most advanced refineries ever built in Brazilian territory. It will be the first with the capability to process 100% heavy crude oil with the minimum environmental impact and to produce fuel with a lower sulphur content than that required by the strictest of international standards, that is to say 10 ppm of sulphur.
Brazil is widely recognised as one of the fastest developing countries of the world, being listed in the BRIC acronym (Brazil, Russia, India and China) as having a rapidly advancing economy. Its population is about 200 million and its land mass makes it the fifth largest country in the world. Rich in natural resources, it also has tremendous potential for hydroelectric power generation.
About WEG
A global major in the power distribution, automation and control sectors, WEG has just celebrated its 50th birthday. The company’s global sales now exceed the US$3-billion mark, representing increasing global success across a wide range of product groups, including the latest generation of transformers, LV control gear, generators, inverter drive systems, soft starters, LV and HV motors, ATEX- compliant explosion proof motors, smoke extraction motors and full turnkey systems. In addition, WEG has recently made a significant strategic expansion of its product portfolio, following the establishment of a joint venture for the manufacturing of wind turbines and the purchase of an Austrian gearbox manufacture, WATT Drive.