Agrolatina, a Peruvian agricultural company specializing in the export of fruits such as grapes, avocados, and pomegranates, has achieved significant improvements in maintenance and industrial performance after implementing WEG’s asset management solution.

Through integrator Inova Chilltec, the company adopted the WEG Motion Fleet Management (MFM) system and WEGscan sensors to monitor the condition of motors and drives in real time. The technology, based on machine learning, provides automatic diagnostics and preventive alerts, enabling assertive decisions and proactive maintenance on the factory floor.

With an initial investment 70% lower than other market solutions, Agrolatina achieved a 100% return on investment (ROI) in just 14 months. Since implementation, operations have continued without critical failures, with increased reliability and efficiency in processes.

WEG’s solution enhanced asset control, improved operational safety, and ensured production continuity — a competitive edge in the international agricultural sector.

About WEG Motion Fleet Management (MFM):

WEG Motion Fleet Management (MFM) is an integrated industrial asset management solution from WEG. Comprising both software and hardware, the solution uses advanced prediction algorithms and IoT (Internet of Things) technology to monitor motors, gearboxes, generators, pumps, compressors, fans, bearings, drives, PLCs, and sensors in real time.

WEGscan sensors collect data on vibration, temperature, and running hours, as well as estimates of speed, load percentage, energy consumption, and output power. This data is sent to a gateway, which automatically transmits it to the cloud, where it can be accessed by maintenance teams through comprehensive vibration reports in the MFM platform.

The solution is widely used in process and manufacturing industries, offering accurate diagnostics and insights to increase asset reliability and availability.

As one of the world’s largest manufacturers of electric motors, gearboxes, transformers, drives, and other industrial equipment, WEG ensures that its customers keep their operations running longer and more efficiently.