WEG Germany has won a major contract from Outotec, the global leader in sulphuric acid plant design and delivery, for a total of 21 MV motors, including slip ring types up to 5200kW, 24 WEG transformers, six liquid rheostat starters, and project management to install and commission the package. The equipment is being installed and commissioned in the World’s largest sulphuric acid production facility, currently under construction at Ras Az Zawr, a mining and industrial city in the kingdom of Saudia Arabia.
Ras az Zawr is a purpose built industrial city/zone on the Arabian/Persian Gulf coast in a region that is one of the richest natural and mineral resources areas in the world. One of the key activities within the Ras az Zawr zone is processing of phosphates for use in fertilisers. This involves phosphate concentrate being processed in a fertiliser production facility, consisting of a phosphoric acid plant, a sulphuric acid production facility, an ammonia plant, a DAP granulation plant and co-generation and desalination plants.
Outotec was successful in winning the contact for the sulphuric acid (SA) segment of the project, the largest production facility of its type in one phase in the World. The total investment in the production facility, which includes three SA plants, is approximately $240M. When complete, the three plants will have a total production capacity of 13,500 tonnes of sulphuric acid per day.
Due to the remoteness of Ras Az Zawr, and the possibilities for issues with multiple suppliers should problems occur, Outotec insisted on single suppliers for each element of the Sulphuric Acid project.
“We didn’t have a previous track record with Outotec in Germany, but we had already done business with the company – successfully - inugh there was no specific reference to this type of plant,” commented WEG General Manager Energy Business, Andreas Schulte M Brazil and Australia, althoesum. “However, our project management single contact, allied with single supplier argument was definitely the key to our winning the bid.”
The project started in 2006, and is only today nearing completion. To-date WEG Germany has supplied 21 Medium Voltage motors: 6 x MAW710 5200kW 4p 13,8kV 60Hz, 6 xMGW450 1400kW 2ph 4,16kV 60Hz, and 9 x HGF400 620kW 6p 4,16kV 60Hz. These motors are used extensively in mining, marine and oil and gas applications; they provide the high levels of efficiency, reliability and long life demanded in the challenging conditions encountered in the Arabian Gulf.
The MGWs and HGF type motors are used in the boiler feed water and circulation pumps of the sulphuric acid plant. The higher power (5,200kW) MAW units are slip ring motors that drive the main blowers in the plant. WEG decided to use slip ring motors controlled by liquid rheostat starters for this application as the blower inertia was large and starting current was an issue. The benefit of starting the main blowers in this way is that the customer can easily control the starting current of the blowers, at the same time handling the very high torques involved.
In addition to the motors and starters, a total of 24 WEG transformers are used to supply and condition electricity to all types of equipment across the whole SA plant, including the WEG MV motors. In common with the MV motors the WEG transformers are designed for use in some of the most demanding operating conditions worldwide in hydro electric plants, desalination systems, oil and gas installations, mining, marine and many more. As evidence of this, WEG recently manufactured and supplied 200-ton transformers – the largest step-up power transformers ever made by the company - for the World’s largest hydroelectric plant, Itaipu Binacional, on the Brazil/Paraguay border.
In terms of project support, WEG was active during the project management stage at Ras Az Zawr, managing three different suppliers, and also co-ordinated with Outotec to ensure that several technical modifications required by the main contractor were actioned promptly and with the required level of customer support. Now that the project is in its start- up phase, WEG is, once again, heavily involved, its co-ordination expertise and technical support being much in demand.
“Once again in a major Global flagship project, WEG has demonstrated its ability to provide a package of key products and the project expertise to integrate them at the highest level,” said Andreas Schulte Mesum, WEG’s General Manager Energy Business. “As a result of this, and other similar successes, no one can deny our credentials as a premier global supplier of integrated supply, control and automation solutions to key commodity markets across the World.”
About Outotec
With more than 600 plants installed worldwide, accounting for over one-third of the current entire global sulphuric acid capacity, Outotec can truly be called the global leader in sulphuric acid plant design and delivery. The company offers vast experience for any acid plant project, whether mini modular at 100 tonnes per day, or mega-sized at 5,000 tonnes or more per day. The scope of Outotec’s services begins with feasibility studies and comprises lump sum turnkey installations with extensive technical support throughout the lifetime of a plant.
About Ras Az Zawr
Ras Az Zawr is a mining and industrial city rising from the sands in the midst of the barren desert and scrub of Saudi Arabia’s Eastern province. At Ras Az Zawr, a phosphate mining, granulation and diammonium phosphate production complex is being built in one stage over a 34-month period, which, upon completion, will be one of the largest integrated phosphate processing and DAP production facilities in the World. Ras Az Zawr is also home to an alumina refinery, aluminium smelter (1066Ha), an 1800MW power station and a downstream industry complex.
About WEG
WEG - one of the worlds largest and most successful manufacturers of electric motors and related control equipment. Specialising in both high efficiency motors and units developed for specific industry applications.